Other Parts Discussed in Thread: SN74LVC1G126
你好:
1、我的SPI总线速度5M,而且长度40cm,想在总线上放一个buffer,请问缓冲器是否需要带施密特输入?
2、我在TI网站找到了带施密特输入的SN74LVC1G17-Q1和SN74LVC1G126,请问在选择哪个更合适?
3、输入带施密特输入和不带的施密特输入的应用场合有什么区别?
4、SN74LVC1G17-Q1的NC引脚是否可以连接到Vcc?这样两个芯片均可以使用。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
1、我的SPI总线速度5M,而且长度40cm,想在总线上放一个buffer,请问缓冲器是否需要带施密特输入?
2、我在TI网站找到了带施密特输入的SN74LVC1G17-Q1和SN74LVC1G126,请问在选择哪个更合适?
3、输入带施密特输入和不带的施密特输入的应用场合有什么区别?
4、SN74LVC1G17-Q1的NC引脚是否可以连接到Vcc?这样两个芯片均可以使用。
您好,
1、信号质量与许多因素有关,这个需要您们自己评估是否需要带施密特输入的buffer;
2、SN74LVC1G126是Standard CMOS输入类型,对输入上升沿和下降沿有要求,具体见参数Δt/Δv 。
SN74LVC1G17-Q1 具有施密特触发输入,没有上升和下降时间限制。
它们都是LVC1G系列的,工作速率可以到160MHZ,速率上都是没问题的。
[FAQ] What is the maximum data rate (or operating frequency) for a logic gate or buffer?
另外,它们的输出类型不同,一个是三态输出,一个是Push-Pull。这需要根据您的应用来决定哪个更合适。
3、对数字信号来说,带施密特输入的抗干扰性更强一些,具体见:了解施密特触发器
4、NC的意思是它内部没有连接到任何东西,因此NC pin 可以连接到任何类型的信号而没有任何问题。