This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,请问一下SN74AVCH8T245,在负载20pf的情况下,可不可以用于给频率100M的信号做电平转换?还有,能支持的最高速率是怎么计算的
您好,
我们是想从1.2V转成1.8V
从1.2V转成1.8V,SN74AVCH8T245 工作频率支持不到100MHZ,如上截图所示,在VCCA ≤ 1.8 V or VCCB ≤ 1.8 V时支持的最大数据速率是170Mbps,也就是85MHZ的信号频率,因此SN74AVCH8T245不支持您的应用。
单位bps是bits per second的缩写,一个信号周期包含2bits,因此它与频率的转换是2倍的关系,即1HZ=2bps。
您具体是应用在什么信号中?看下下面FAQ是否可以解决您的问题,或者说明您的应用我再看是否有TI其他芯片推荐给您。