This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2T45: 电平转换前级输入和级输出波形不一致。

Part Number: SN74LVC2T45


HI  TI的工程师
最近使用你们一款电平转换芯片遇到一个问题(芯片型号:SN74LVC2T45)
问题描述:
我的应用场景是使用在SPI电平转换上面的(FLASH),SPI_MISO,CS ,CLK 这3个信号都没有问题,但是SPI_MISO信号 3.3V 转换为1.8V,输入输出存在差别,蓝色为输入信号(3.3V)黄色为输出信号(1.8V),
A到B这段时间输入信号是存在不确定电平状态,输入信号完全拉低至0V输出信号才拉低的,导致A-B这段时间时间从机SPI_MISO发送给主控的信号有误,请问可能是这么导致的?

对此我有几个疑问: 

1,SN74LVC2T45这款芯片的输入端高低电平的阈值的多少?和芯片规格书一致吗?规格书描述高底电平是:

VIH min = VCCA × 0.7 V, VIL max = VCCA × 0.3 V。

实际波形和电路图如图所示:




  • 1,SN74LVC2T45这款芯片的输入端高低电平的阈值的多少?和芯片规格书一致吗?规格书描述高底电平是:

    输入高低电平阈值和datasheet中描述是一样的,如果VCC在4.5V和5.5V之间,Vih(min)=0.7Vcc 是没问题的。3V 供电的话Vih=2V。

    SPI_MISO的信号频率为多大?