This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0206: 用作eMMC5.1电平转换

Part Number: TXS0206


Hi,experts

 我想用TXS0206这颗芯片来做eMMC5.1的1V8到3V3的电平转换芯片,位宽为8bit,可否帮忙看下采用2pcs TXS0206的电路这样设计是否有问题,速度可否达到60Mhz?十分感谢!

  • 您好,TXS0206首先适用于SD卡的应用,1.8V到3.3V转换clock的频率最高为60Mhz,data rate达到60Mbps。

    如果使用8通道,两颗这样应用我觉得是可行的,注意就是输入和输出走线尽量等长保证一定的输出延迟。

    另外,对于第二颗不用的引脚,CLKA是CMOS输入不建议直接悬空,建议上拉或下拉到固定的逻辑电平,CMDA/CMDB内部已经上拉所以可以直接悬空。

    CLKB和CLKf都是输出端,也可以直接悬空。