如果 我给OE低电平 此时VCCB侧为高阻
在这个状态下 VCCB侧 的输入输出口的逻辑电平可以大于6.5V吗
我想TTL和RS232共用连接器,通过OE电平和RS232芯片的使能来切换逻辑电平
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
首先6.5V是芯片引脚可以承受的最大绝对值电压,而不是芯片功能性测试的最大电压哈,我们在使用芯片时需要参考的是Recommended Operationg Conditions,因此可以看到Vcc的最大电压是5.5V而不是6.5V,输入引脚的最大电压也是VCC即5.5V。那当OE为低电平时,输入端的电压可以为0~5.5V,但是此时输出端是高阻态的。