in the datasheet, both the VIL of the power A/B sid is 0.15V(max), for example, if we use the chip for I2C levelshift, if the low logic higher than 0.15V in B side, what is the logic in A side? I think if B side high than 0.15V, the chip could not recongnize the signal as "LOW" logic in cornern case, so that the output in the A side, it will show as "high " logic? thanks.