This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G126: 3.3V输入电平转移

Part Number: SN74LVC1G126

Hi ti,

需要将串口的3.3V CMOS TX信号转为1.8V或2.5V电平输入到SOC里;

请问用SN74LVC1G126的话,VCC连接2.5V时,TX信号输入到A口,是否能在Y实现2.5V的信号输出?

VCC连接1.8V时,TX信号输入到A口,是否能在Y实现1.8V的信号输出?