Part Number: SN74AVC4T774
使用SN74AVC4T774器件,A端接1.8V供电,B端接3.3V供电,A→B输出接口配置,B端负载有4.7K下拉电阻测试电平幅值异常,请问输出端是否可以连接上下拉电阻?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74AVC4T774
使用SN74AVC4T774器件,A端接1.8V供电,B端接3.3V供电,A→B输出接口配置,B端负载有4.7K下拉电阻测试电平幅值异常,请问输出端是否可以连接上下拉电阻?
您好,根据数据手册,3V供电时,Iol sink电流为12mA时,可以下拉到最大0.7V低电平,相当于最多下拉50ohm。所以使用4.7Kohm下来肯定会导致电平异常的,最好不加电阻才能拉下来。

顺祝,中秋国庆双节快乐
你好 Kallyn ,Iol的 这里的说明 3V 供电,驱动电流达到 12mA 是无法拉低的,最低为 0.7V,增加4.7K下拉电阻以后为什么无法拉高呢,怎么解释呢?对地 4.7K最多只有 0.7mA的驱动能力,为什么会拉不高呢?
Iol的 这里的说明 3V 供电,驱动电流达到 12mA 是无法拉低的,最低为 0.7V
是低电平最高为0.7V呢。
所以计算下来下拉是50ohm,强下拉。
如果使用4.7Kohm的话,电压是拉不下来的,所以您测试的结果是低电平异常。