This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108: 驱动能力问题

Part Number: TXB0108
Other Parts Discussed in Thread: SN74LXC8T245

您好!我开发了一台SWD协议的烧录器。单片机PA5引脚和PA1引脚分别对应SW_CLK和SW_DIO。我使用TXB0108将单片机输出的3.3V信号转换为5V信号为芯片烧录程序。通信时钟频率为1MHZ。烧录器与芯片之间的连接线长度大于40cm时,就无法正常烧录。请问这种情况我该如何改进硬件设计?能否推荐一款驱动能力更强的自动换向双向电平转换器?

  • 您好,

    您还是需要8通道的吗?看下SN74LXC8T245

    如果需要2通道的看下SN74LVC2T45

    4通道的没有自动方向转换的推荐给您,看您有DIO应该需要双向电压转换。

    或者把您需要的通道需求再说明下吗?方向控制型电压转换芯片您考虑吗?