Other Parts Discussed in Thread: SN74AXCH1T45
您好,请问如图所示的将SN74AXCH2T45做成双向转换电路的方案是否可行,SN74AXCH2T45电平转换芯片在1.8V转1.8V时的速率是多少呢?SN74AXCH1T45电平转换芯片在1.8V转1.8V时的速率是多少呢?想要的是1.8V转1.8V时的速率达到300Mbps以上
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请问如图所示的将SN74AXCH2T45做成双向转换电路的方案是否可行,SN74AXCH2T45电平转换芯片在1.8V转1.8V时的速率是多少呢?SN74AXCH1T45电平转换芯片在1.8V转1.8V时的速率是多少呢?想要的是1.8V转1.8V时的速率达到300Mbps以上
将SN74AXCH2T45做成双向转换电路的方案是否可行
可行的,控制引脚DIR的高低电平决定了传输方向,当DIR=L时, 从B port到A port传输,当DIR=H时,从A port到B port 传输。
SN74AXCH2T45电平转换芯片在1.8V转1.8V时的速率是多少呢?SN74AXCH1T45电平转换芯片在1.8V转1.8V时的速率是多少呢?想要的是1.8V转1.8V时的速率达到300Mbps以上
通常在计算这类器件能支持的传输速率时,可以通过传输延迟的倒数来进行评估,比如VCCA=VCCB=1.8V时,tpd(max)=7ns。
所以1/7ns=142.86Mbps. 所以300Mbps的速率是达不到的。

您好,AVC系列的是能够支持较高速率的电平转换器件,datasheet中给出了下面几种速率,但是1.8V到1.8V的tpd我看了下大概在4ns左右,评估的话差不多在250Mbps左右。我的建议是可以少买几片实际验证下,因为根据下面的速率参考以及tpd的估算300Mbps的余量不是很大,所以建议实际验证下。