This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1T45: 电平转换芯片可以用在高速脉冲信号上面吗?

Part Number: SN74LVC1T45
Other Parts Discussed in Thread: SN74AVC1T45, SN74AXC1T45

请问一下SN74LVC1T45这颗芯片能否用于高速脉冲信号上面?

脉冲宽度8ns,电压3.3V,能否用电平转换芯片来将电压转换为1.8V?

谢谢!

  • 您好,

    如下 SN74LVC1T45 datasheet 首页特性描述,支持3.3V与1.8V间电压转换,最大速率75Mbps,即37.5MHZ,周期是26ns,脉冲宽度是13ns,因此脉冲宽度8ns是不支持的

    您可以看下SN74AVC1T45和SN74AXC1T45

  • 您好,

    我在6.8节看到了这组参数,上升时间和下降时间和约28ns。这个应该就是脉冲信号最小需要的宽度了吧?

    另外,您说的数据转换率75Mbps,为什么对应的频率是37.5MHz呢?一个周期内应该只有一个bit的数据吧?

    谢谢!

  • 我在6.8节看到了这组参数,上升时间和下降时间和约28ns。这个应该就是脉冲信号最小需要的宽度了吧?

    可以这样估算;

    另外,您说的数据转换率75Mbps,为什么对应的频率是37.5MHz呢?一个周期内应该只有一个bit的数据吧?

    bps 是bit per second,即每秒的位数,信号的频率是一秒变化的周期数,一个周期包含高低两种状态,即用2bit 表示,所以说1HZ是2bps,是2倍的关系,因此75Mbps对应的频率是37.5MHz。

    一个周期内应该只有一个bit的数据吧?

    一个周期2bits,一个周期包含高和低两种数字状态,需要用2位去表示。

  • 好的,懂了,谢谢解答!