Part Number: TXS0102
TXS0102接UART信号,VCCA和VCCB都是3.3V,VCCA是常供电,VCCB休眠时断电,休眠时VCCB这边的IO是否会有电?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXS0102
TXS0102接UART信号,VCCA和VCCB都是3.3V,VCCA是常供电,VCCB休眠时断电,休眠时VCCB这边的IO是否会有电?
您好,您说的这个现象即为逻辑器件大多数都支持的Ioff(也称为partial power down" 或者 "back-drive protection.)特性,也就是我们担心的倒灌问题,Ioff的目的就是倒灌保护。同样TXS0102也有这个特性,

当VCC=0时,Ioff特性使得IO处于高阻抗状态。在这种高阻态下的最大漏电流可以参考数据手册的Ioff,参考关于Ioff特性的FAQ:。


在TXS0102的应用手册中也提到:当VCC power down时,输出为disable的, 这样便能放置输出端倒灌电流回到电路中。
https://www.ti.com/lit/an/scea044/scea044.pdf

不客气,后续有其他问题,大家再一起讨论。
顺祝元旦快乐。