管脚描述中,OE参考VCCA电压,要求VCCA≤3.6V。从 “6.3 建议运行条件”中看,OE最大电压可以到5.5V。
当前我的设计中,VCCA=1.8V,VCCB=3.3V,OE采用3.3V电平控制,不知道是否可以,是否会存在漏电问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
管脚描述中,OE参考VCCA电压,要求VCCA≤3.6V。从 “6.3 建议运行条件”中看,OE最大电压可以到5.5V。
当前我的设计中,VCCA=1.8V,VCCB=3.3V,OE采用3.3V电平控制,不知道是否可以,是否会存在漏电问题?
您好,
首先提醒你查看最新版的datasheet,如下产品首页链接,如下截图中包含中英文datasheet,因为我看你的截图是 “6.3 建议运行条件”,而我在官网看到的是“5.3 建议运行条件”
https://www.ti.com.cn/product/cn/TXS0108E
对于你的问题,答案是可以,具体解释见下面FAQ:[FAQ] Can I connect the OE pin to Vccb supply pin instead of Vcca for TXS, TXB devices?