Part Number: SN7406
关于结温:
请问规格书中有记载Ta最大值70℃,理解为工作时最大的环境温度,那么它的结温规格是多少呢?

关于ICCL:
规格书中记载最大值为51mA,是指6通道同时工作时,还是单一通道工作时呢?

谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
最大结温是 150 °C, 具体见 [FAQ] What is the maximum junction temperature (TJMAX) for a device?
ICCL是所有通道输出为低电平时的供电电流。