This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC4T245RSVR

Part Number: SN74AVC4T245RSVR


SN74AVC4T245RSVR UQFN16 2 CHANEL DUAL-BIT 2.6*1.8mm -40~85℃
  该芯片没有数据传输时,目前发现4PCS有漏电流大的问题,具体情况如下:
  第1片:漏电流约0.2mA。
  第2片:漏电流约2mA。
  第3片:漏电流约2mA。
  第4片:漏电流约20mA。

我们这边排查了外围电路:
① 245的第1/16脚由拉低改为拉高(不使能)
② 断开信号引脚 A/B的信号连接,直接上拉/悬空
③ 断开其他所有引脚,只保留第2、3、10、11脚,也即是仅接了该芯片的供电部分。
以上的修改后测试,漏电流还是一样的大,没有任何改善。