Other Parts Discussed in Thread: TXB0304
hi 你好,使用LSF0108进行1.2V和3.3V电平信号转换,用于QSPI信号双向通信,目标速率是50MHz,但当速率提高到50MHz会出现写入数据和读取数据不一致的问题,目前实测最大速率只能支持到33.33MHz时数据和读取数据是一致的,参考电路图如下,实测时A侧的上拉是去掉的,为了增大驱动能力B侧的上拉换成了330Ω,还请看下什么原因导致的速率提高到50MHz时出现写入数据和读取数据不一致。

50MHz时写入数据和读取数据不一致:

33.33MHz时CKL和DQ0的波形如下: