This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G74: 应用和配置问题

Part Number: SN74LVC1G74

用SN74LV1G74这个片子,输入为100M CLK,原来参考的项目是输出了50M的差分时钟,现在有2个问题

第一,输出差分的模式,我理解应该是Q接CLK_P,nQ接CLK_N

第二,这个片子我看也有单端的接法,如果SN74LV1G74用单端输出的话,那输出的CLK频率是多少?我现在的需求是想输出一个单端50MHz的CLK,但没看到有配置的地方

  • 您好,

          nQ与Q输出同频,相位相差180°。

         只用Q端的输出,即为单端信号。

         由于此芯片是在CLK上升沿触发,当频率为100MHZ的的时候,输出50MHZ.。