This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC245A: 类似芯片推荐

Part Number: SN74LVC245A

Hi,我在手册中看到F28388D controlCARD的GPIO支持的是3.3V的LVCMOS电平标准,不支持5V的电压输入,于是我在5V的TZ保护信号和控制卡之间增加了一个TSSOP封装的SN74LVC245A,想起一个电平转换的功能,但是由于电平转换的芯片我给了5V的VCC供电,在实际测试中发现并没有起到电平转换的功能,经过LVC245芯片输出的信号电压仍然在5V。

想问下有没有相同封装的电平转换芯片,能在5V的供电下,将5v的信号转成3.3V的信号呢。

非常感谢您的帮助!