This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104: 双向电平转换芯片出现问题。

Part Number: TXB0104


电路图如下:

问题描述:B端口给stm32上串口使用,A端口给FPGA使用,目前B端口的UART2_TX和UART2_RX两个引脚输出电平到A端口,其中UART2_TX输出信号可以被FPGA检测到,但是UART2_RX输出信号不能被FPGA检测到。

以上B端口驱动引脚UART2_TX和UART2_RX在stm32上设置的都是推挽输出,FPGA上两个引脚配置模式都是一样的(UART2_RX这一个端口电压拉低只能到1.4V的样子,不能完全拉低),很奇怪的现象。