This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G07: SN74LVC2G07

Part Number: SN74LVC2G07


如果Vcc=5.2,

输入端1A/2A接单片机普通IO口3.3v

输出端1y/2y接上拉10k电阻,

请问此时如果单片机输出高,1y2y是什么状态,电压多少?0v还是5v还是其他值

谢谢


  • 感谢您对TI产品的关注!
    关于你的咨询,VCC 5.2V的话, Vin 3.3V是个临界状态。
    介于高电平和低电平之间。
    无法明确出输出电平。
    最好将SN74LVC2G07的VCC调整到3.3V。
    来确保3.3V input在高电平范围内,输出高电平。