This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0204: 能否使用LSF0204实现1.2V和1.8V信号之间的电平转换

Part Number: LSF0204


从datashee 首页可以看到,LSF0204支持1.2V和1.8V的信号电平互转。如下图所示:

但是从datasheet 的page14可以看到:建议Vrefb的电压比VrefA的电压高1V以上,如下图所示:

我的问题是:LSF0204是否支持1.2V和1.8V信号之间互相转换?