This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: TXS0102的输入电源如果是DCDC,,会改变电压值

Part Number: TXS0102


TPS563201DDCR按照推荐电路设计输出电压3.3V,但是当3.3V电压接入TXS0102的VCCA,会导致DCDC输出电压偏高,从3.3V变成3.49V

  • 您好

    首先,咱们得确认一下TPS563201DDCR的功率电感饱和电流是否足够。你得确保这个电流至少是输出峰值电流的1.3倍以上,这样才能保证稳定的输出电压。

    其次,检查一下layout布局是否合理,特别是功率路径回路,要尽量小,以减少损耗和干扰。

    再者,确认一下输入电压是否稳定且符合规格要求。TPS563201DDCR的输入电压范围比较宽,但还是要确保它在合适的范围内,别太低也别太高。

    另外,TXS0102的VCCA电压范围是1.65V到3.6V,虽然3.49V还在这个范围内,但接近上限了。你得确认一下这个电压是否会对TXS0102的工作产生影响,或者是否存在其他可能影响电平转换的因素。