This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
At present, it is necessary to use this device to realize the level conversion of 10ns pulse width 30KHz refrequency pulse signal, and the output impedance inside the SN74LV245A device needs to be known.
problem:The output impedance of SN74LV245A after OE is enabled is required.
Hi ruchan,
With a 4.5 supply, the worst-case output impedance is VOL / IOL = 0.55 V / 16 mA ≈ 34 Ω. The typical value is roughly half that.