Part Number: TXS0108E
工程师你好,
我们目前选用TXS0108EPWR芯片,用来将1.8V的信号和3.3V的信号进行相互转换。
目前芯片的VCCA接1.8V,VCCB接3.3V。
请问VCCA与VCCB的两个电源,有没有上电时序的要求呢?
感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
没有上电时序要求,但是VCCA > VCCB时VCCB存在的泄漏电流。设计电路时要注意此点。
Note:TXS0108EPWR支持部分断电模式应用,其中VCCA和/或VCCB断电且电压为0V,从而导致输出被禁用,并最大限度地减少流经器件的电流回流。
详情请阅读下面的tech report。
Biasing Requirements for TXS, TXB, and LSF Auto-Bidirectional Translators