This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC4245A: VCCA接的5V,VCCB接的3.3V,占空比为50%的时候A脚输出的不是2.5V?

Part Number: SN74LVC4245A

DIR ,OE都是直接接的单片机引脚并是低电平,发现从B1给到的PWM波占空比为50%,测量A1电压为0.68V;而不是2.5V?帮忙看看是什么原因?通过示波器接到A1是有正常波形输出的