This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] XTR117:2线/3线情况下的 XTR117

Guru**** 2810265 points

Other Parts Discussed in Thread: XTR117, XTR111, XTR115, XTR116

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1078029/xtr117-xtr117-in-a-2-3-wire-situation

部件号:XTR117
线程中讨论的其他部件: XTR111XTR115XTR116

您好,


XTR117是否可以在2/3的电线环路情况下使用。 目标是设置一个跳线,例如在2线和3线之间切换。

在2线情况下,XTR117按照数据表中的说明进行连接。

在3线情况下,导线(引脚3)断开,电路的其余部分连接到3线接地端。

这有可能吗? 有什么影响?

如果不可能,是否有解决这种情况的办法? XTR111是否可能实现这一点?


谢谢!


此致

斯蒂芬