请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:LMH6559 我们计划在~1.2 GHz频率下运行LMH6559。
是否需要缓冲器电路以避免在大于1 GHz时与输出发生杂散耦合?
谢谢。
jp
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Jehangir:
如果你只是计划缓冲500MHz到1GHz -40dBm的噪声频谱,它位于0-1.8V低频时钟信号的顶部,那么我认为 在 直流耦合模式和+/-5V电源下运行LMH6559应该是可以的。 但是,我不认为LMH6559适合在500MHz到1GHz频段中处理大信号(>0.4Vpp)。 我认为您不会特别需要大于1GHz的缓冲器电路,因为缓冲器频率的滚落应该会处理超出该部件-3dB带宽的任何脉冲。
此致,
Rohit