This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] XTR115:XTR115的电流输出来自外部电源或电压输入?

Guru**** 2575035 points
Other Parts Discussed in Thread: XTR115, XTR111

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/565168/xtr115-current-output-of-xtr115-drawn-from-external-supply-or-voltage-input

部件号:XTR115
主题中讨论的其他部件: XTR111

你(们)好

我的应用使用XTR115将0-5V从模拟输出卡转换为4-20mA

模拟输出卡最多可输出1 mA

因此,我想知道:
XTR115是从外部电源获取电流,还是从0-5V信号获取电流?

提前感谢您的参与

此致
Petter