This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LMV393:开关功能VIN < 300mV

Guru**** 2519070 points
Other Parts Discussed in Thread: LM393

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/612681/lmv393-switching-functionality-vin-300mv

其它部分在线程中讨论:LM393HiJian

我使用的是LM393的备用部件,开关功能也有类似的问题。
即使VIN小于300mV (参考电压),比较器也在切换输出状态。

情况如下:

参考电压(针脚3)设置为2.530v
当VIN (针脚2)的2.324v比Vref设置的值低200mV时,输出将切换为低电压。


比较器由3.3V供电
参考电压通过简单的分压器电路产生。

为什么会发生这种情况?