This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] OPA627:作为基于PCM1794A的耳机放大器/DAC中的差分放大器

Guru**** 2553450 points
Other Parts Discussed in Thread: OPA1644, BUF634, OPA627, PCM1792A, OPA1622, OPA1612, OPA1688

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/611603/opa627-as-a-difference-amplifier-in-pcm1794a-based-headphone-amp-dac

部件号:OPA627
主题中讨论的其他部件:OPA1644BUF634PCM1792AOPA1622OPA1612OPA1688

我有兴趣使用OPA627 (可能还有BUF634)作为我的DAC/耳机放大器的输出级。  我计划使用OPA1644作为跨阻抗放大器,将 来自PCM1792A DAC的电流转换为差分电压,此信号转换为单个OPA627 (左右各一个) 配置为差分放大器,增益为1,将信号转换为信号结束信号,以驱动一对耳机(50欧姆至600欧姆)。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    David,
    虽然OPA627肯定可以用于此应用程序,但您可能还需要考虑使用OPA1612,OPA1622或OPA1688作为耳机驱动程序。 即使在32欧姆负载中,这三种产品都具有出色的THD+N规格,并且在600欧姆时与OPA627的THD+N相匹配或超过。 OPA1622可能最适合此应用程序,但仅在VSON封装中可用,而其它两个则在SOIC中可用。