This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] OPA693:使用5V单电源时OPA693混合/最大电源工作范围

Guru**** 2943430 points

Other Parts Discussed in Thread: OPA693

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/616151/opa693-opa693-mix-max-supply-operating-range-when-5v-single-supply-use

部件号:OPA693

大家好,

OPA693单电源范围是5V至12V。
当客户使用5V单电源(典型)时,是否需要保证OPA693操作的最小/最大电源?
如果是最大电源,则在12伏以下正常工作,但最小电源如何?
我们是否可以保证4.8V单电源或4.5V单电源?
您是否会让他们知道在5V以下可接受的瞬态电源电平?
谢谢你。

此致,
Jade