This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] THS4531:使用Vocm引脚在FDA中设置输出电压

Guru**** 2826755 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/614671/ths4531-setting-the-output-voltage-in-a-fda-using-vocm-pin

部件号:THS4531

大家好,

在我关于使用FDA将IQ调制解调器连接到IQ调制器的最后一篇文章之后:
我需要将我的输出通用电压调整为1.4V左右,而FDA的IQ输出以3.3V/2 =~1.65V为中心。
我想知道我是否可以使用一个简单的电阻器并联到分压器底部电阻器,而不是将1.4V的外部直流电源连接到Vocm引脚?
谢谢大家,
David