请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:INA220
大家好,
1.客户希望使用INA220监控150A电流。
2.电流感应电阻器是2512封装,额定功率为1W至3W。
您能否帮助查看原理图,并确认这些电阻器比率足以进行150A监测?
谢谢!
SHH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.