请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:INA326 我正在使用INA326放大来自负载单元的信号,Vdd=3.3V,我要设置输出电压wrt VDD/2,(考虑负载单元在两个方向上的移动)。 在数据表中,建议的电路如图2所示。 但使用此电路时,输出电压为954mV。根据图1,在平衡条件下,输出完全为VDD/2 (正确)。
那么,哪个电路(图1或图2)是正确的电路?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Vishal,
图2中的电路是2000 的正确电路,其工作正常-参见下文。 检查您的连接或修改此帖子中所附的示意图。