请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TL074 在我的应用中,Tl074输出将具有一个拉高电阻器2k到5V和0.1uF到GND。
根据测试结果,输出电压信号和增益是正确的。
但是,当我使用这些高拉电阻2k和Cap 0.1uF进行运算放大器输出时,是否存在任何风险?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.