This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TLV8811:整个温度范围内的最大偏移电压

Guru**** 2551630 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/636714/tlv8811-max-offset-voltage-across-full-temperature-range

部件号:TLV8811

最大偏移电压仅指定为25°C

40 °C至125°C整个温度范围内的最大偏移电压是多少?