请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:INA129 客户的电路也很好,他们最关心CMRR。
测试输入为VCM=10V@10Hz,VDIFF=100uV@10Hz。
输入自IN+和IN-,CMRR >119dB; 但输入自IN+和IN-,CMRR <80dB。
客户的要求是如何在输入IN+和IN-时使CMRR大于110dB。
谢谢,新年快乐!
Marc
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.