请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:INA826 INA826作为增益为50的电流感应放大器进行布线。 偏置电压为+5V和-4.5V。 我对输入放大器的输入应用了50mV直流。 我期望0.01uF电容器的电压为2.5VDC。
我没有收到任何信号。 我错过了什么? 谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.