Other Parts Discussed in Thread: OPA350
您好,几个有关使用OPA350的问题,谢谢!
1.对于将OPA350用于DCDC转换器的电流感应放大器是否有任何问题 ,如下所示。 OPA350数据表典型应用不包括电流感应放大器,因此我很担心。

2.如果按此方式配置,并且增益配置为20,则可用带宽是多少。 增益-带宽-产品的定义是开环,但这是闭环,所以我感到困惑。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Shengnan,
请问您能不能这样善良地回答这些问题?
Kai
请参阅下面我的答案:
1. 大多数运算放大器(包括OPA350)可用于电流感应,只要输入电压不违反运算放大器的线性输入共模电压范围。 此外,R1/R2的值应比Rsense高得多,以便最大程度地减少由流经输入电阻器而不是Rsense的一些电流引起的错误-因此,仪表放大器可能比差分放大器更好。
话虽如此,若输入电压可能会高于/低于电源电压0.3V,输入电流应限制在10mA或更低,以防止ESD保护二极管受损(例如使用串行输入电阻器)。 顺便提一下,请注意,如果上述MOS开关的Ron电阻与Rsense相当,则可能会引入显著的测量误差。
2. 应用程序的带宽BW是闭环增益的函数,GCL:BW = GBW/GCL,其中GBW是增益-带宽产品(OPA350为38MHz)。 因此,对于20的增益中的OPA350,有效带宽约为1.9MHz -请参阅下面的模拟。