This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] THS4631DGNEVM:直流偏压至放大器或输入

Guru**** 2589265 points
Other Parts Discussed in Thread: THS4631DGNEVM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1095995/ths4631dgnevm-dc-bias-voltage-to-the-amplifier-or-inputs

部件号:THS4631DGNEVM

大家好,  

将THS4631DGNEVM用作增益为2的同相放大器。 我正在发送一个-5V至+5V的信号,该信号将放大至-10+10V。 但是,我还想添加一个直流偏压,以便输出信号为0V至20V。 我无法将偏置信号添加到输入波形,因此我尝试查看是否有方法将直流偏置电压添加到放大器或输入(例如,叠加放大器配置)以实现此目的。

谢谢你。