This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LMV358:输出异常

Guru**** 2914580 points

Other Parts Discussed in Thread: LMV358

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1104058/lmv358-output-exception

部件号:LMV358

 您好,TI

问题描述:

板载运算放大器lmv358idr的输出异常,与规格不一致(全刻度输出仅为4.5V,无法达到VCC电源附近的5V电压)

特定验证方法:

1. TW1和TW2之间存在开路。 此时,通过2K电阻将运算放大器引脚5的输入上拉至VCC2 (5V)。 此时,针脚7输出的理论值应为5V-20mV = 4.98v,实际测试仅为4.6V左右。 大约有10块电路板被测试,这种现象是一致的。

2.当TW1和TW2之间连接固定电阻时,当输出电压低于4.6V时,输入和输出均无问题。 当输入超过4.6V时,输出已饱和,不会随输出的增加而增加。

3.使用Tina模拟回路,模拟结果没有问题。