This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] OPA693:1:8模拟扇出驱动器:

Guru**** 2668255 points

Other Parts Discussed in Thread: OPA692, OPA3692, OPA693, OPA3693

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1114814/opa693-1-8-analog-fanout-driver

器件型号:OPA693
主题中讨论的其他器件:OPA692OPA3692OPA3693

我想制作一个具有 扇出模拟信号1:8的电路。

OPA692的第一页显示电路符合我们的要求,仅采用2*OPA692

最近、我发现 OPA3692有3个通道、也许我可以实现如下所示:

但我有2个问题:

(1)

数据表中 OPA3692 (3CH)和 OPA692 (1CH)的输出电流均为190mA

OPA692使用190mA、没问题。

 OPA3692是每通道190mA 还是每通道190mA/4?

(2)

我还发现 OPA693具有类似配置、但它仅驱动2通道(数据表)

OPA693的最大输出为120mA、约为 OPA692的一半。

因此、我想驱动"足够"的电流、每个输出通道应该为50mA。

(50 Ω 端接电缆和 RG316电缆)

对吧?