This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TLV8811:LTSpice 仿真错误

Guru**** 2555630 points
Other Parts Discussed in Thread: TLV8811, TINA-TI

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/989633/tlv8811-ltspice-simulation-error

器件型号:TLV8811
主题中讨论的其他器件: PSpice for TITINA-TI

您好!

我正在尝试在 LTSpice 中模拟以下电路。 它只是用于进一步仿真的测试电路。

我从以下页面下载了.lib 文件: https://www.ti.com/product/TLV8811#design-development##design-tools-simulation
遗憾的是、当我尝试使用 TLV8811时、我始终会收到以下错误消息:

Warning: Multiple definitions of model "outputcir_vohvol_dideal" Type: Diode
Warning: Multiple definitions of model "outputcir_isc_dideal" Type: Diode
Warning: Multiple definitions of model "recoverycircuit_dideal" Type: Diode
Warning: Multiple definitions of model "vinrange_dideal" Type: Diode
ERROR: Node U1:I0:I21:1:102 is floating and connected to current source G:U1:I0:I21:1:RA
ERROR: Node U1:I0:I19:1:102 is floating and connected to current source G:U1:I0:I19:1:RA
ERROR: Node U1:I0:I19:1:302 is floating and connected to current source G:U1:I0:I19:1:RC

u1:vpd: Missing value, assumed 0V @ DC
u1:i0:vprobe2: Missing value, assumed 0V @ DC
u1:i0:vprobe1: Missing value, assumed 0V @ DC
Direct Newton iteration failed to find .op point. (Use ".option noopiter" to skip.)
Starting Gmin stepping
Increasing initial diagonal Gmin to 100
Gmin = 100
vernier = 0.5
vernier = 0.25
vernier = 0.125
vernier = 0.0625
Gmin = 75.2941
vernier = 0.03125
vernier = 0.015625
vernier = 0.0078125
vernier = 0.00390625
Gmin = 73.2748
vernier = 0.00195313
vernier = 0.000976563
vernier = 0.000488281
Gmin = 0
Gmin stepping failed

Starting source stepping with srcstepmethod=0
Source Step = 3.0303%
Source Step = 33.3333%
Source Step = 63.6364%
Source Step = 93.9394%
Source Step = 100%
vernier = 0.015625
Source Step = 99.9882%
Source stepping succeeded in finding the operating point.


Date: Mon Mar 29 10:17:53 2021
Total elapsed time: 0.654 seconds.

tnom = 27
temp = 27
method = modified trap
totiter = 4748
traniter = 2093
tranpoints = 1029
accept = 1027
rejected = 2
matrix size = 182
fillins = 363
solver = Normal
Thread vector: 28.8/11.0[4] 2.7/2.4[2] 8.8/3.8[4] 1.1/0.9[3] 2592/500
Matrix Compiler1: 21.84 KB object code size 12.1/6.3/[5.0]
Matrix Compiler2: off [2.3]/4.8/2.5

我希望有人可以帮助我解决这个问题。 我不知道如何解决这个问题。

谢谢、此致