主题中讨论的其他器件: LM7705
您好!
我正在尝试在 TINA 中模拟 INA333电路、它看起来不工作。
我的输入正弦波的最小值/最大值设置为0 - 13mV。 根据数据表、增益电阻器为1.1k 时、增益应约为92。 如下面的屏幕截图所示、输出不符合预期(应为正弦波、最小/最大偏移为0 - 1.96V、偏移为200mV。
我出了什么问题?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、Wilson、
您超出了 INA333的共模输入电压范围。 与电源轨保持至少0.1V 的距离:
e2e.ti.com/.../wilson_5F00_ina333.TSC
因此、您的信号在 INA333的输出上已经是错误的。
Kai