This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 用于测量0至20mV 电压的汽车级精密放大器

Guru**** 2774995 points

Other Parts Discussed in Thread: AMC1301-Q1, AMC1311-Q1, INA333-Q1

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/885363/automotive-grade-precision-amplifier-for-measuring-0-to-20mv

主题中讨论的其他器件:AMC1301-Q1AMC1311-Q1INA333-Q1

尊敬的团队:

我们需要测量单端0至20mV 信号、Pls。 建议使用-40至+125°C 精密仪表放大器的良好汽车级。我们将使用内置16位单端 ADC 的 MCU、ADC 参考电压为+2.5V。

我计划使用 AMC1311-Q1或 AMC1301-Q1进行隔离。我能否将传感器直接连接到 AMC1301-Q1精密隔离放大器、然后将差分输出转换为单端输出、或者首先需要使用仪表放大器进行放大、然后将其提供给 AMC1311-Q1

谢谢、此致

Ravi Chawda