This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] OPA320:在电源低于规格的情况下使用 OPA320。 (1.71V)

Guru**** 2584205 points
Other Parts Discussed in Thread: OPA320, LM7705

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/928875/opa320-use-of-opa320-with-power-supply-below-spec-1-71v

器件型号:OPA320
主题中讨论的其他器件: LM7705

OPA320的额定工作电压范围为1.8V 至5.5V、温度范围 为-40至125。

   如果温度范围 设置为 0至70,是否可以使用低至1.71V 的电源电压?

此致

Tor Dag