This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] INA333:增益不是预期值

Guru**** 2931100 points

Other Parts Discussed in Thread: INA333

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/928858/ina333-gain-is-not-as-expected

器件型号:INA333

您好!

我将使用 INAEVM-MSOP8以以下配置测试 INA333。 V+=2.5V、V-=-2.5V。 REF = 0V、RG = 1K、这将设置增益= 100。

尽管 IN-未连接到 GND、但我测量的共模电压仅为0.6mV。

IN+-IN-、 OUT=112mV

3mV 111.1mV

6mV 111.4mV

9mV 111.6mV

然后、我尝试从 IN+- IN-从1mV 到10mV、OUT 始终大约为112mV。

这里出了什么问题?