请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM321 主题中讨论的其他器件: LM7705、 OPA341、 TLV341、 LMV611、 TLV2211
您好!
我正在搜索与 LM321相同的封装和引脚排列、但在0V 输出电压下具有更大的灌电流(>5mA)。
此致、Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.