This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] THS3001:压摆率限制

Guru**** 2503735 points
Other Parts Discussed in Thread: THS3001

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1214037/ths3001-slew-rate-limiting

器件型号:THS3001

大家好、我相信 Michael 将会回答此问题、但当 THS3001在 x2.5和 x4增益下使用时、我会尝试获得最快的稳定时间。 数据表上引用的5倍增益为25-75%时压摆率、0-25%和75-100%可能慢得多。 我的问题是、当未发布25-75%以外的值时、如何避免全尺寸步长的压摆率限制? 例如、我可以很好地将输入转换限制为对应于200V/us、这增加了100%的裕度、但我敢断定、仍然不足以防止转换率限制、例如10%- 0%、因此0.1%的稳定时间可能会混乱。 我在 THS3001数据表上的注释是、它仅用于单位增益、不表示用于测试的源的输入压摆率。

TI 是否有任何其他信息、我想假设必须提供用于测试的源的压摆率?

此外、转换速率指定为5倍增益、在 x1增益下稳定。 TI 是否有稳定时间与增益的关系图? 如果不仅仅是 x2.5、x4和 x5的值也会非常有用。

谢谢、Steve