This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TLV1701-Q1:解决方案建议

Guru**** 2818575 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1251826/tlv1701-q1-solution-recommendation

器件型号:TLV1701-Q1

大家好、

您能帮助找到适合以下应用的合适解决方案吗?

输入信号:10Hz PWM、电压范围为0V 至18.5V

输出信号:当  VIL:0~2 V 时、逻辑低电平;逻辑高电平=  VLH:4.2-18.5V

此致、

东宝市